Please note that the item you have bought is a 115V.

Positive Displacement Blowers | Raptor Supplies Worldwide

Positive Displacement Blowers

Filter

Positive displacement blowers are used in wastewater treatment, pneumatic conveying, vacuum systems, food processing and energy production applications to offer a constant flow of air or gas from one ... Read More

SPEEDAIRE -

Positive Displacement Blowers / Vacuum Pumps, 4 Inch FNPT

Speedaire positive displacement blowers, are also known as rotary lobe blowers. These blowers pull air into an inlet port and capture it with the help of rotating lobes that force the air to move forward. These blowers offer high volumes of air through a pipe or hose to a required location and are capable of working at higher vacuum levels in comparison to regenerative blowers. Choose from a range of these displacement blowers, available in 1.5 and 2.5 inch FNPT outlet diameters.

StyleModelCFM RangeDisplacementMax. PressureOverall DepthOverall HeightOverall WidthRPM RangePrice (ex. VAT)
A2EPR8209 to 5420.210 cu. ft./rev.13 psi10.375"16.6"18.38"1070 to 2850$4,465.74
B2EPR9388 to 9530.350 cu. ft./rev.7 psi15.375"11.94"22.38"764 to 2850$4,778.31
SPEEDAIRE -

Positive Displacement Blower/Vacuum Pump, Inlet Dia.: 2.5" (F)NPT Outlet Dia.:

StyleModelRPM RangeCFM RangeDisplacementShaft Dia.Shaft LengthKeyway WidthMax. PressureOverall DepthPrice (ex. VAT)
A2EPT2764 to 2850134 to 3590.140 cu. ft./rev.1.125"2.5"0.25"15 psi15.375"$4,250.31
B2EPP61091 to 3600108 to 3500.104 cu. ft./rev.0.75"2"0.187"7 psi11.25"$2,710.35
SPEEDAIRE -

Positive Displacement Blower/Vacuum Pump, Inlet Dia.: 3" (F)NPT Outlet Dia.: 3

StyleModelRPM RangeCFM RangeDisplacementShaft Dia.Shaft LengthKeyway WidthMax. PressureOverall DepthPrice (ex. VAT)
A2EPT8637 to 2350152 to 4770.227 cu. ft./rev.1.375"2.94"0.312"15 psi18"$6,762.64
B2EPR3955 to 3600197 to 5790.170 cu. ft./rev.0.875"2.375"0.187"7 psi12.375"$3,372.40
SPEEDAIRE -

Positive Displacement Blowers

Speedaire blowers / vacuum pumps are used in different industrial applications, such as wastewater treatment, surface cleaning, pneumatic conveying and dairy milking. They feature superior-strength cylinder with heat-dispersing fins. They also have high-temperature seals offering leak-free operation, decreased noise and low vibration levels. Choose from a range of these blowers / vacuum pumps, available in 1.5 and 2.5 Inch FNPT inlet diameters.

StyleModelCFM RangeDisplacementInlet Dia.ItemMax. PressureOutlet Dia.Overall WidthPrice (ex. VAT)
A2EPP2---Blower---$2,458.23
B2EPR7---Blower---$4,465.74
C2EPU3---Blower---$13,057.31
D2EPR4---Blower---$3,275.46
D2EPT3---Blower---$4,250.31
E2EPR2---Blower---$3,170.54
F2EPP7---Blower---$2,710.35
C2EPU5---Blower---$10,524.30
A2EPP8---Blower---$2,486.91
G2EPU6---Blower---$10,524.30
G2EPU4---Blower---$13,057.31
G2EPT7---Blower---$9,178.05
H2EPU2---Blower---$11,303.29
I2EPP9---Blower---$2,486.91
H2EPT5---Blower---$7,187.20
D2EPT1---Blower---$4,778.31
G2EPT9---Blower---$6,762.64
I2EPP5---Blower---$2,561.79
F2EPP3---Blower---$2,427.70
I2EPP1---Blower---$2,188.15
J2EPU1---Blower---$11,303.29
C2EPT6---Blower---$9,223.04
J2EPT4---Blower---$7,187.20
D2EPR6---Blower---$2,980.05
K2EPR572 to 2180.069 cu. ft./rev.1.5" (F)NPTPositive Displacement Blower/Vacuum Pump15 psi1.5" (F)NPT13.92"$2,980.05
StyleModelRPM RangeCFM RangeDisplacementShaft Dia.Shaft LengthInlet Dia.Outlet Dia.Overall DepthPrice (ex. VAT)
A2EPP41091 to 360057 to 1860.060 cu. ft./rev.0.75"2"2" (F)NPT2" (F)NPT11.25"$2,529.99
A2EPN91389 to 527522 to 730.017 cu. ft./rev.0.625"1.97"1" (F)NPT1" (F)NPT9.25"$2,188.15

Features

Speedaire Blower Vacuum Pumps

  • They have a cylinder with heat-dispersing fins for added strength.
  • These pumps feature high-temperature seals for leak-free operation, low vibration levels and reduced noise.

Speedaire Displacement Blowers / Vacuum Pumps

  • These blowers pull air into an inlet port and capture it using rotating lobes that force the air to move forward.
  • They offer high volumes of air through a pipe or hose to a required location and can work at higher vacuum levels than regenerative blowers.

Working Mechanism

  • The blower is powered by an electric motor or an engine, which drives a pair of rotors or lobes that rotate in opposite directions within a housing.
  • As the lobes rotate, they create a sealed chamber between themselves and the housing. The volume of this chamber decreases as the lobes move towards the outlet, causing the air or gas to be compressed.
  • At the outlet side of the blower, the compressed air or gas is discharged into the system. The volume of the chamber increases as the lobes move towards the inlet, creating a low-pressure area that allows more air or gas to enter the blower.
  • The cycle keeps repeating and the lobes keep trapping & compressing a fixed volume of air or gas and releasing it at the outlet.

Frequently Asked Questions

Can Speedaire positive displacement blowers be used in hazardous environments?

Yes, Speedaire positive displacement blowers can be designed and manufactured for use in hazardous environments. They can be constructed with explosion-proof motors and other safety features to comply with industry standards and regulations.

How do I maintain these displacement blowers?

  • Regularly inspect and clean the inlet and outlet ports to prevent debris or contaminants from entering the blower.
  • Check the drive belt or coupling for wear and adjust the tension or alignment as needed.
  • Inspect the seals for leaks and replace them if necessary.
  • Change the oil or lubrication as recommended by the manufacturer. The frequency of oil changes will depend on operating conditions and usage.
  • Inspect the cooling system, if applicable and clean the heat exchangers or radiators to ensure proper cooling.
  • Monitor the temperature and vibration levels of the blower and address any abnormal readings promptly.
  • Keep a log of maintenance activities and inspections to track the blower's performance and identify any potential issues.

How do I install these displacement blowers?

  • Determine the location for the blower. It should be installed in a well-ventilated area with adequate space for maintenance and inspection.
  • Ensure that the foundation or mounting surface is level and can support the weight of the blower.
  • Connect the inlet and outlet ports of the blower to the piping system using appropriate fittings and connections. It is important to use the correct size and type of piping to prevent pressure drops and ensure optimal performance.
  • Install the motor or engine that will power the blower. Make sure it is properly aligned and securely mounted to prevent vibration and excessive wear.
  • Check and adjust the belt tension or coupling alignment, if applicable, to ensure smooth operation.
  • Fill the blower with the recommended type and amount of lubrication.
  • Test the blower, ensuring it operates within the specified parameters.
  • Install any necessary accessories or controls, such as filters, silencers or pressure gauges, according to the manufacturer's instructions.
  • Label the blower with its model number, operating specifications and maintenance requirements for future reference.

We are here to help!

Looking for a part not listed here?