Blind Rivets(758 Products)
1/4" Closed End (6 items)
1/4" Lockbolt Break-Pins (7 items)
1/4" Open End (89 items)
1/8" Closed End (38 items)
1/8" Open End (178 items)
13/64" Open End (3 items)
15/64" Open End (1 item)
17/64" Open End (2 items)
3/16" (2 items)
3/16" Closed End (34 items)
3/16" Lockbolt Break-Pins (3 items)
3/16" Open End (230 items)
3/32" Open End (13 items)
5/16" Open End (5 items)
5/32" Closed End (22 items)
5/32" Open End (103 items)
6.3mm Open End (1 item)
6mm Open End (1 item)
9/32" Open End (1 item)
Miscellaneous Blind Rivets (21 items)
Description
Blind rivets or break stem rivets are designed to install fasteners where there's no access to the rear end of the joint. They are used in assembling applications ranging from small electronic components to gigantic steel beams. Raptor Supplies offers a wide range of blind rivets from Grainger, Stanley, Westward, Hanson, POP, Disco, & more. The tubular construction allows the mandrel to easily pass through the centre. Choose from a wide range of multi-grip, structural, split and TriBulb rivets on Raptor Supplies.
Features
- Blind rivets are made of two parts: the rivet body / shell / hat and the setting mandrel within it.
- Both the hat and the mandrel come pre-assembled and ready for use.
- These rivets require only one side of the installation surface to be accessible, making them easy to install with a rivet gun or hand riveter.
Frequently Asked Questions
What is the difference between open-end blind rivets & closed-end blind rivets?
- Open-end blind rivets are made from fine-grade materials to ensure consistent, error-free application from rivet to rivet.
- Closed-end blind rivets provide complete mandrel retention, which increases the tensile strength of the sealed rivet. They are useful in electronic and electrical applications.
How to measure a blind rivet?
- Determine the diameter of the rivet using a dial calliper or measuring gauge.
- Measure from the underside of the rivet head to the end of the rivet head, excluding the mandrel.
- The measured length will be 1.5 times the grip range of the rivet (including the ball at the end of the rivet).
How to install a blind rivet?
- Drill a hole and insert the rivet into the hole.
- The mandrel is pulled against the hat of the rivet by a tool.
- The back of the mandrel has a bulge on one end or is connected to the hat in some way, causing the hat's edges to expand down towards the material.
- When this expansion exerts pressure on the material, a designed fault in the mandrel reaches its maximum force capacity and snaps, leaving a properly installed rivet in place.