Anchor Screws(479 Products)

Description

Anchor screws are fasteners used to attach objects to walls, ceilings or other surfaces that may not be strong enough to support the object's weight on their own. Raptor Supplies offers a wide range of these anchor screws from brands like Dewalt, Powers Fasteners, Red Head, Strong-Tie, Tapcon, Grainger, Diversified Fastening Systems, Vestil and Vigil Antislip.

Features

  • They have a threaded shaft and a head that can be driven into the surface using a screwdriver or drill.
  • These screw-in anchors require no pre-spotted holes.
  • They resist vibration and can be used in both cracked or uncracked concrete.
  • These steel oval head concrete screws feature zinc / black oxide finish for corrosion resistance and durability.

Frequently Asked Questions

What is the difference between an anchor screw and a regular screw?

An anchor screw provides a secure hold in materials that may not be able to support the weight of an object on their own. Regular screws are designed to hold objects together.

How to choose the right anchor screw for my project?

Choosing the right anchor screw depends on the weight of the object being attached, the type of surface it will be attached to and the environment it will be installed in.

How do I install anchor screws in concrete?

Installing anchor screws in concrete involves drilling a hole into the concrete and then inserting the anchor screw.

How do I ensure that anchor screws are installed correctly?

Ensure that the anchor is appropriate for the job, the hole is drilled to the correct depth & diameter and the anchor is installed correctly.

What is the anchor length of these screws?

These screws are available in 1/2 to 10-inch anchor length variants.

What is the difference between stainless steel hex slotted concrete screws and steel pan head concrete screws?

Stainless steel hex slotted concrete screws feature a hexagonal head with a slotted drive for easy installation with a wrench or screwdriver, while the steel pan head concrete screws feature a rounded, slightly domed head for even load distribution and a flush finish upon installation.