A Complete Guide to Digital Panel Meters

Digital Panel Meters are commonly used in industrial control panels to measure physical quantities like temperature, pressure, voltage, current, power and speed accurately. They offer various benefits, such as linear display, high accuracy, ease of calibration and the ability to store configuration parameters. Let’s understand the functionalities, types, applications and essential considerations for the selection

Read More

How to Use Dissolved Oxygen Meters?

A dissolved oxygen (DO) meter measures the concentration of oxygen dissolved in water, which is essential for aquatic organisms’ survival. It finds applications in environmental monitoring to assess water quality, ensuring suitable conditions for aquatic life. Additionally, in wastewater treatment plants, it monitors oxygen levels to ensure effective treatment processes. To take an accurate measurement

Read More

Introduction to Dissolved Oxygen Meters

Dissolved oxygen meters are indispensable tools for measuring the crucial parameters of oxygen dissolved in water. They serve a critical purpose in monitoring the health of aquatic environments. These meters are ideal across diverse industries and applications, including environmental science, aquaculture and wastewater treatment. Environmental researchers rely on them to assess water quality and ecological

Read More

AMS 317.04 Regular Auger

AMS 317.04 regular auger is a companion for precise and effective soil sampling with diverse soil types or challenging conditions. Also, it can be suitable for drilling to increased depths, where distinct soil samplers or soil core samplers come into play. So, whether you’re conducting geological surveys, environmental studies or agricultural research, this auger proves

Read More

Thomas 270047 Articulating Piston Compressor

Thomas 270047 Articulating Piston Compressor is used for a compact and reliable air source. Also, it has articulating piston technology for smooth and efficient operation. This compressor is ideal for medical, laboratory and industrial settings to provide a consistent air supply for pneumatic devices, maintaining precision and reliability in critical applications. Features Get amazing deals

Read More

Avoid Parallax Error in Gauge Readings

One thing that matters the most during any measurement is accuracy. Whether it is during manufacturing applications or scientific research, nobody likes errors. Also, when it comes to pressure gauge measurements, one common challenge is parallax. Parallax errors can compromise accuracy. This error will, in turn, lead to inaccurate results. If you want to ensure

Read More

Makita 1002BA Curved Base Planer

Makita 1002BA curved base planer is ideal for working on scarves made of logs and for shaping arcs and arches out of timber. The tool is often used to give timbers and logs a hand-hewn appearance by making a small adjustment to the blades. Features Working Mechanism Makita 1002BA Curved Base Planer Raptor Supplies can source any

Read More