Introduction:
Hydraulic jack makes lifting heavy loads a breeze and is a cornerstone tool for both professionals and DIY enthusiasts. They are particularly useful for automotive repairs, construction, and various industrial applications. In this blog post, we will delve into the functionality, usage and maintenance of hydraulic jacks.
How Does a Hydraulic Jack Work?
To lift heavy objects, a hydraulic jack exerts pressure on a fluid contained in a closed system. Pascal’s principle transmits this pressure in all directions, amplifying the force to lift the object. This active process facilitates easier lifting of heavy objects using the jack.
- The hydraulic jack comprises a chamber filled with hydraulic fluid.
- Within the chamber, a plunger or piston is capable of moving up and down.
- When force is applied to the plunger, it exerts pressure on the hydraulic fluid.
- Pascal’s principle comes into play by transmitting pressure to the chamber’s walls.
- The distribution of pressure creates a force that lifts the piston for lifting the load.
Types of Hydraulic Jack:
Here is some information about various types of jacks that are suitable for different industries. It is crucial to ensure that the jack is used safely and correctly.

Bottle Jack
Named for its resemblance to a milk bottle, bottle jacks operate using a vertical shaft pumped with a hand lever. They are ideal for the automobile industry to lift cars and are known for their ability to fit in small spaces.
Scissor Jack
Scissor Jacks are smaller in size and easy to store. It operates by lifting the weight with a lead screw and tightening the linkages with a small crank. Scissor jacks are useful for changing tyres on cars and vehicles. Also, they tend to operate relatively slow and are somewhat lightweight.


Floor Jack
Floor jacks operate vertically. When you push down the handle, the floor jacks lift the object upward vertically. There are two types of floor jacks: mechanical and hydraulic. Mechanical floor jacks use a screwing mechanism to lift weight. On the other hand hydraulic floor jacks use check valves, cylinders and pistons to do the job. Moreover, the main advantage of floor jacks can sit low to the ground and operate quickly.
Hi-Lift Jack
Hi-Lift Jacks are used for farming vehicles rather than cars or trucks. They were designed by the Bloomfield Manufacturing Company over 100 years ago. Hi-lift jacks use two climbing pins that work alternatively to lift the weight. One pin holds the load while the other is freed and moved to the next hole while lifting.


Trolley jack
Trolley jacks are designed to lift a vehicle to allow for repair or regular maintenance. They are designed to lift vehicles and hold them in a safe position for a short period. Also, the wheels of a trolley jack can make slight movements for shifts in the car.
How to Use a Hydraulic Jack:
Notably, it’s important to follow procedures to ensure safety while using a hydraulic jack. Here’s a step-by-step guide on how to use a hydraulic jack:
- Choose a hydraulic jack that can handle the weight of the load you intend to lift.
- Subsequently, place the jack on a stable and level surface to prevent instability.
- Moreover, identify the designated jacking points on the vehicle or equipment.
- Utilize the pumping handle to raise the load slowly for even strokes.
- Once the load reaches the desired height, place the jack stand under it to provide support.
- When finished release the pressure on the hydraulic jack and lower the load.
How to Fill a Hydraulic Jack:
Maintaining the hydraulic fluid in your jack is essential for its optimal performance. So, here’s a simple guide on how to fill a hydraulic jack:
- Most hydraulic jacks have a fill plug located on the chamber’s side or top.
- Initially, use a wrench or socket to remove the fill plug.
- Carefully pour hydraulic fluid into the chamber until it reaches the recommended level.
- Once the chamber is filled, then tighten the fill plug for a proper seal.
If you’re looking for a wide range of hydraulic jack options, Raptor Supplies has got you covered. We are a global MRO supplier with an extensive catalogue of over 2 million products to choose from. You can get in touch with our 24×7 chat support or reach out to us via phone, WhatsApp or email at any time. Also, feel free to check out our dedicated review page to see what our valued customers have to say about our service.