Authorized Distributor ofTAP MAGIC

TAP MAGIC

Tap Magic aluminium cutting fluids are designed for cutting and machining operations on aluminium, brass, copper and other soft metals without stains on the surface of a workpiece. These aluminium cutting fluids are ozone-friendly and completely free of 1, 1, 1 trichloroethane, ideal for achieving a micro-fine finish. They are available in cans, pails and drums having a maximum capacity of 275 gallons. Tap Magic offers bio-degradable ProTap cutting fluids for drilling, tapping, milling or cutting on any metal while not staining or changing the properties of even soft metals, such as aluminium. These fluids offer rapid heat dissipation, closer tolerances and ultra-fine finish, regardless of the cut.

See More

Request a Quote

TAP MAGIC Penetrants and Lubricants

Penetrants and Lubricants (7 Products) Recommended for adding a coating or slippery film on machinery, tools & parts for reducing friction & wear between surfaces and ensuring smooth running of equipment. Can be applied to hinges & bearings to limit overheating or squeaking noises

About TAP MAGIC

Tap Magic aluminium cutting fluids are designed for cutting and machining operations on aluminium, brass, copper and other soft metals without stains on the surface of a workpiece. These aluminium cutting fluids are ozone-friendly and completely free of 1, 1, 1 trichloroethane, ideal for achieving a micro-fine finish. They are available in cans, pails and drums having a maximum capacity of 275 gallons. Tap Magic offers bio-degradable ProTap cutting fluids for drilling, tapping, milling or cutting on any metal while not staining or changing the properties of even soft metals, such as aluminium. These fluids offer rapid heat dissipation, closer tolerances and ultra-fine finish, regardless of the cut.

Major Trade Names

Tap Magic H2O NC

Tap Magic H2O NC

It offers great lubricity while removing the unpleasant, sticky coating typical of products containing heavy oils. It is suitable for non-ferrous metals, typically for aerospace or military applications that do not allow chlorinated lubricants.

Tap Magic EP-Xtra

Tap Magic EP-Xtra

Tap Magic EP-Xtra features an ozone-friendly formula that offers superior performance on all cuts and all metals. The patented additive, EP-Xtra, provides a synergistic boost in performance.

Tap Magic Eco-Oil

Tap Magic Eco-Oil

It is redeveloped to meet the requirements of NSF's H1 Food Grade certification. It has a natural oil base that is significantly low in odour and smoke, even on cuts that generate a lot of heat.

Frequently Asked Questions

Q. Can we use Tap Magic on aluminium?

A. When working with aluminium, brass, copper and other soft metals, Tap Magic Aluminum is the cutting fluid of choice. It won't leave a stain on the surface of the piece unlike some other fluids on soft metals. The finish is usually outstanding and the precision is always excellent.

Q. Who makes Tap Magic?

A. The Steco Corporation has been involved in designing and producing the world's greatest industrial cutting fluids since 1953. Tap Magic product line has become the most frequently known name in cutting fluids, offering superior precision, greater lubrication and the best protection for valuable tools.

Q. Is Tap Magic Eco-Oil made of petroleum?

A. Tap Magic Eco-Oil has been redeveloped to meet the requirements of NSF's H1 Food Grade certification. It is biodegradable and features a natural oil base that's exceptionally low in odour and smoke, even on cuts that generate a lot of heat.

Q. How do I store Tap Magic cutting fluids?

A.

  • Store Tap Magic cutting fluids in a cool, dry place, away from direct sunlight & other heat sources.
  • Tightly seal the container to prevent evaporation and contamination.
  • Store it in an upright position to avoid spilling.
  • Keep the fluid away from sparks, flames and any ignition sources.

Q. How do I apply a Tap Magic cutting fluid?

A.

  • Clean the surface to be cut.
  • Shake the bottle well before use.
  • Apply a small amount of cutting fluid directly onto the cutting surface or tool.
  • Reapply if required during cutting to maintain lubrication & cooling.
  • Follow the brand's instructions & safety warnings before using cutting fluids.

Q. How does Tap Magic inhibit corrosion?

A. Tap Magic corrosion inhibitors form a protective layer on metal surfaces to prevent corrosion caused due to moisture, chemicals and other environmental factors.