Authorized Distributor ofSTARRETT-UK

STARRETT-UK

Starrett manufactures measurement instruments, PRECISION tools AND hand tools. The company's precision tool range includes micrometres, callipers, rulers, protractors, levels, gages, dial indicators, surface plates, squares and vises. The Starrett micrometre catalogue comprises a wide variety of mechanical, digital / electronic, depth and inside micrometres, which are used to measure dimensions in 1-inch increments to 0.0001-inch accuracy. Starrett also manufactures Vernier, dial, digital and spring callipers for taking measurements in the metalworking, forestry and woodworking industries. Starrett dial indicators translate small linear distances into rotational movements. They are available in graduations ranging from 0.001 mm to 0.01 mm in the metric system and from 0.00005 inches to 0.001 inches in the imperial system. Starrett miter protractors are used for direct & comparative measurement of angles and are available in manual, digital, miter & universal-bevel variants. These tools are widely used by machinists, toolmakers and quality inspectors for setting bevels, transferring angles or checking cutter clearances. Choose from a wide range of these Starrett tools, including hardness testers & tachometers, on Raptor Supplies.

See More

Request a Quote

Load More

Things To Consider

Shipping

These Starrett tools are small in size and require compact packaging. Hence, they are delivered in packs consisting of several pieces. These tools are suitable for courier shipment and not air freight.

About STARRETT-UK

Starrett manufactures measurement instruments, PRECISION tools AND hand tools. The company's precision tool range includes micrometres, callipers, rulers, protractors, levels, gages, dial indicators, surface plates, squares and vises. The Starrett micrometre catalogue comprises a wide variety of mechanical, digital / electronic, depth and inside micrometres, which are used to measure dimensions in 1-inch increments to 0.0001-inch accuracy. Starrett also manufactures Vernier, dial, digital and spring callipers for taking measurements in the metalworking, forestry and woodworking industries. Starrett dial indicators translate small linear distances into rotational movements. They are available in graduations ranging from 0.001 mm to 0.01 mm in the metric system and from 0.00005 inches to 0.001 inches in the imperial system. Starrett miter protractors are used for direct & comparative measurement of angles and are available in manual, digital, miter & universal-bevel variants. These tools are widely used by machinists, toolmakers and quality inspectors for setting bevels, transferring angles or checking cutter clearances. Choose from a wide range of these Starrett tools, including hardness testers & tachometers, on Raptor Supplies.

Frequently Asked Questions

Q. How accurate are Starrett dial indicators?

A. Dial indicators convert linear distances into rotational movement that measures dimensions up to 4 inches, with an accuracy of 0.0001 inches. They are usually mounted to a magnetic base or another Starrett fixture.

Q. How do you read a Starrett dial indicator?

A.

  • Mount your dial indicator on a stand.
  • Turn the outer dial face until the hand points to 0.
  • Begin displacing your spindle.
  • Check for errors at half revolutions.
  • Begin to reverse your revolutions.
  • Take five measurements of the same item.
  • Look at the faces on your dial indicator.
  • Measure how long your spindle is.
  • Identify measurement marks.
  • Press the spindle against the item to be measured.
  • Count the marks displaced on the small gauge & calculate the measurement.
  • Count the marks displayed on the large gauge & calculate the measurement.
  • Take both these gauge measurements and add them.

Q. How do you calibrate a Starrett micrometer?

A. Place the setting bar between the measuring faces. Once the ratchet clicks, gently turn the thimble. Turn the sleeve gently until the thimble zero and sleeve index are aligned, and place the spanner in the hole. The Starrett micrometer is now calibrated.

Q. What is the difference between the graduations on an outside micrometer and a depth micrometer?

A. Both regular outside and depth micrometers have the same spindle and graduations, but the graduation order for depth micrometers is reversed. Digital depth micrometers have better resolution than conventional line-graduated depth micrometers.