Sign In

SPEEDAIRE

1...45...2

Things To Consider

Cross-Reference Alternatives

Some Speedaire tools cross individual references to the equivalent Ingersoll Rand model numbers. So, if you're looking for a competitor tool that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Speedaire tool available.

Shipping

These Speedaire tools range from small to large sizes. They may require careful packaging as some tools may get damaged while shipping. Hence, these Speedaire tools are delivered by courier shipment and air freight for minimum downtime.

About Speedaire

Speedaire, a Grainger brand, offers a wide variety of high quality pneumatic tools and equipment. Its product line includes compressors, pressure switches, pneumatic cylinders and compressed air filters that are designed to perform under high pressure conditions. Speedaire pneumatic air cylinders are ideal for applications where a magnetic sensing piston is not required. These compact cylinders feature stainless steel construction to withstand temperatures ranging between -40 & 200 degrees F and pressure up to 200 psi. These pneumatic cylinders have an end cap made of aluminium to provide high thermal efficiency and have silver finish to ensure excellent solderability. Speedaire air regulators are designed for controlling the input pressure in air lines of pneumatic tools. These compressed air tools feature zinc / aluminium construction for resisting corrosion on exposed surfaces and to withstand pressure up to 450 psi. These Speedaire air regulators deliver a maximum flow rate of 2000 cfm and are available in lengths ranging from 4 to 13.25 inches.

Speedaire Competitive Advantages

Speedaire Auto Drain Valves

Speedaire Auto Drain Valves

These auto drain valves are ideal for draining condensed water & oil from filters, aftercoolers, moisture separators, dryers and air receiver tanks. These timed electric drain valves come equipped with an adjustable electronic timer for automatic opening & closing of valves. These Speedair...

e auto drain valves feature a filter ball valve for controlling high pressure flow rates and reducing frictional losses. Models from the 38X Series, such as 38XT33 & 38XR59, can handle temperatures ranging from 35 to 95 degrees F, while models from the 13X Series, such as 13X524, 13X525, 13X526 & 13X528, have an operating temperature range of 14 to 140 degrees F.

Frequently Asked Questions

What is a timer drain valve?

Timer operated drain valves are reliable and cost effective valves that periodically open the drain's valve for a specific amount of time. The valve may be open for a few seconds every hour for the removal of the collected condensate.

What is an auto drain?

An automatic drain is a 2/2 valve that closes when the system is subjected to a particular pressure. The drain opens when liquid gets accumulated and allows the float to rise on depressurisation.

How do auto drain valves work?

Auto drain valves allow condensate to settle down into the condensation reservoir of the valve. When the liquid present in the reservoir rises up to the point where seats get lifted by the float, controlled air pressure is sent to the pneumatic piston for opening the typically closed 3/4 ported ball valve.

Are Speedaire timed electric auto drain valves dust proof?

Yes, Speedaire timed electric auto drain valves come equipped with an IP65 rated enclosure to provide excellent dust resistance.

Should you leave your air compressor drain valve open?

Ideally, you should drain the moisture tank after each day's use. If the unit remains unused for a while, it is recommended to leave the drain valve open till the time it is used next. This will help moisture to drain out completely and also resist corrosion on the inner surface of the tank.

What is the pressure handling capacity of Speedaire timed electric auto drain valves?

Speedaire timed electric auto drain valves are capable of withstanding pressures ranging from 250 to 4000 psi.

What happens if the air compressor is not drained?

If air compressors are not drained properly, the drain will rust up and not be functional after a while. The tank will also get filled with water instead of air, and water will flow out of the air hose.