Sign In

PROTO

123...2

Things To Consider

Cross-Reference Alternatives

Proto Tools torque wrenches (manufacturer's part numbers) generally cross individual reference to the equivalent AMPCO Metal model numbers. So, if you are looking for a competitor torque wrench that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Proto torque wrenches available. Customers can also cross-reference most of these couplings using the last five digits of the model numbers.

Shipping

These Proto torque wrenches and steel crowfoot wrenches are small in size and require compact packaging. Hence, they are delivered in packs consisting of several pieces and are suitable for courier shipment and not air freight.

About Proto

Proto Tools catalogue includes a wide range of sockets, wrenches, ratchets, screwdrivers, hex keys, pliers, snips, clamps, master sets, punches, chisels and tethered tools. Proto torque wrenches, also known as digital torque wrenches, provide a precise torque reading by measuring turning force electronically to avoid over tightening of fasteners. These wrenches are commonly used to apply consistent torque on assembled products for safety and quality control applications. They feature a digital display with visual alerts & an audible buzzer for delivering accurate torque output. Proto socket sets feature TorquePlus configuration with radius-corner design for shifting the stresses away from the corners and uniformly distributing over a large surface area. The internal design of these sockets further reduces rounding of the edges and offers more flexibility to turn worn out or rusted fasteners. Choose from a wide range of these quality wrenches & other company products, such as socket bits, hand-held punches & chisels on Raptor Supplies.

Major Trade Names

Proto SkyHook Tools

Proto SkyHook Tools

Proto SkyHook tools include dock pocket kits, switch connectors, apron kits, bolt bag kits & saddle kits. Proto tools & storage units provide safe tethering & transfer of tools for various industrial applications. Selected models offer synthetic construction for ease of maintenance.

Proto SkyDock Attachments

Proto SkyDock Attachments

Proto SkyDock attachments include various wrist straps and tool storage attachments. The SkyDock attachments are used in conjunction with SkyHook pocket kits for securely anchoring to the belt, wrist, apron or the station. Users can easily replace / switch the anchoring type with hand-to-hand, perso...

n to station, hand to belt or person to person configuration.

Proto Compo-Cast hammers

Proto Compo-Cast hammers

Proto Compo-Cast combo face hammers feature urethane construction for preventing the hammer from damaging the workpiece. This construction ensures that the hammer retains its shape even after striking on sharp edges and hard surfaces. Its dual-head design (slim line head & standard dead blow head) e...

nsures that the hammer meets the application requirement.

Proto Clik-Stop adjustable wrenches

Proto Clik-Stop adjustable wrenches

Proto Clik-Stop adjustable wrenches have a locking design for securely holding their moving jaws in place when in operation. Proto wrenches have a square jaw opening for providing tight fit and strength. The extra-wide jaw capacity ensures that the wrench can accommodate various applications.

Proto Facom safety gloves

Proto Facom safety gloves

Proto Facom safety gloves protect the user against sharp objects and blow in various industrial applications. These safety gloves have silicon leather to provide complete mechanical protection near machinery and heavy tools. These gloves are designed to easily fit over latex insulating gloves for en...

suring user comfort and safety. Users can safely handle Proto hand tools with these safety gloves.

Proto Stanley SortMaster organiser

Proto Stanley SortMaster organiser

Proto Stanley SortMaster organisers are ideal to store small parts & tools for transportation. Proto tool sets feature lid structure for preventing the movement of small parts & tools from one compartment to another. They have removable dividers for easily customising the compartments depending upon...

the tool / part size. Their additional latch design enables back to back organiser stacking for storage efficiency.

Proto Competitive Advantages

Proto Facom insulated ratchets

Proto Facom insulated ratchets

Proto Facom insulated ratchets are ideal for fastening nuts and bolts for applications prone to electrical leakage. These Proto professional tools have two colour warning handle insulation that changes colour to yellow if the insulation integrity is compromised during the operation. They have a spring ball tip for securing the sockets & accessories...

while fastening.

Frequently Asked Questions

Which tools are offered by Proto?

Proto offers various tools, including storage units, hand sockets, drive tools, impact sockets, wrenches, pliers, clamps, snips, screwdrivers, hex keys and torque wrenches.

What is the difference between a socket wrench and a ratchet?

Socket wrenches are designed to fasten nuts & bolts. However, these tools are not ideal for tight spaces as they need to be lifted after each fastening cycle. Whereas, ratcheting wrenches have pawls that enable the wrench to spin in one direction while turning the bolt in another.

Can the standard / regular sockets be used with impact wrenches?

No, regular sockets should not be used with impact wrenches. These sockets are likely to shatter against the power of impact wrench because of their thin wall design and construction material.