Authorized Distributor ofMAIN FILTER INC.

MAIN FILTER INC.

Main Filter's extensive catalogue includes interchange hydraulic filters, pressure line filters, return line filters and filter systems. The brand's transmission filter kits have a collapse pressure of 101 psi, with a corresponding cracking pressure also set at 101 psi. These filters feature a glass filter media and are rated at 25 microns for enhanced protection for minute particles. They come with a Viton gasket for a robust sealing mechanism. Main Filter interchange hydraulic filters feature wire mesh as their filter media, with a filter rating of 200 microns. They can be operated in an inside-out flow direction and can handle a diverse range of fluids, including HH, HL, HM and HV for versatile fluid compatibility. These filters can withstand and strain contaminants up to 200 microns.

See More

Request a Quote

Product Categories

MAIN FILTER INC. Hydraulic Filters

Hydraulic Filters(78017 Products)

MAIN FILTER INC. Filter Systems

Filter Systems(103 Products)

Things To Consider

Cross-Reference Alternatives

Raptor Supplies offers a complete range of Main Filter products. We can recommend suitable products for your diverse application requirements. Raptor Supplies offers a complete range of Main Filter products. We can recommend suitable products for your diverse application requirements.

Why Us?

These Main Filter products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these Main Filter items are delivered by courier shipment and air freight for minimum downtime.

About Main Filter Inc.

Main Filter's extensive catalogue includes interchange hydraulic filters, pressure line filters, return line filters and filter systems. The brand's transmission filter kits have a collapse pressure of 101 psi, with a corresponding cracking pressure also set at 101 psi. These filters feature a glass filter media and are rated at 25 microns for enhanced protection for minute particles. They come with a Viton gasket for a robust sealing mechanism. Main Filter interchange hydraulic filters feature wire mesh as their filter media, with a filter rating of 200 microns. They can be operated in an inside-out flow direction and can handle a diverse range of fluids, including HH, HL, HM and HV for versatile fluid compatibility. These filters can withstand and strain contaminants up to 200 microns.

Frequently Asked Questions

How do I clean hydraulic filters by Main Filter?

  • Turn off the hydraulic system and relieve pressure.
  • Locate and remove the hydraulic filter housing cover.
  • Carefully take out the used hydraulic filter from its housing.
  • Inspect the filter for visible contaminants and damage.
  • Clean the filter housing using a lint-free cloth or compressed air.
  • If the filter is reusable, clean it by tapping off excess dirt or using compressed air from the inside out.
  • Replace the hydraulic filter with a new one if it is not reusable or shows signs of damage.
  • Securely reattach the hydraulic filter housing cover.
  • Turn on the hydraulic system and check for leaks.

What is the difference between the brand's interchange hydraulic filters and interchange hydraulic pressure line filters?

  • The brand's interchange hydraulic filters remove contaminants from the hydraulic fluid. They are positioned in the hydraulic system to filter fluid before it reaches components like pumps. Whereas, the brand's interchange hydraulic pressure line filters are used to filter fluid within the high-pressure lines of a hydraulic system. They are installed in the pressure line to capture particles before they reach critical components, such as actuators or cylinders. These filters protect high-pressure components from damage and wear.