Sign In

Authorized Distributor of

ENPAC

The company's product line includes drums, spill pallets, portable spill containment products and storage and dispensing products. Enpac's salvage drums are designed to store and transport damaged or leaky containers with hazardous liquids and substances. They are made of high-density polyethylene (HDPE) material that is resistant to corrosion and chemical degradation. They have an open-head design with a screw-on lid that provides easy access to the contents of the drum. This design also allows for easy loading / unloading of hazardous materials, as well as easy cleaning and maintenance of the drum. The brand's water-filled diverters help to divert or contain liquids in the event of a spill or leak and can be drained and folded for convenient storage when not in use. They are ideal for use in stormwater management, portable washdown / pressure washing diversion, spill diversion and equipment decontamination.

See More

Request a Quote

ENPAC

Things To Consider

Cross-Reference Alternatives

Enpac MPNs cross individual references to the equivalent Justrite, Eagle and Romold model numbers for transport drums and spill containment systems. So, if you're looking for a competitor item that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Enpac products available.

Shipping

These Enpac products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.

About Enpac

The company's product line includes drums, spill pallets, portable spill containment products and storage and dispensing products. Enpac's salvage drums are designed to store and transport damaged or leaky containers with hazardous liquids and substances. They are made of high-density polyethylene (HDPE) material that is resistant to corrosion and chemical degradation. They have an open-head design with a screw-on lid that provides easy access to the contents of the drum. This design also allows for easy loading / unloading of hazardous materials, as well as easy cleaning and maintenance of the drum. The brand's water-filled diverters help to divert or contain liquids in the event of a spill or leak and can be drained and folded for convenient storage when not in use. They are ideal for use in stormwater management, portable washdown / pressure washing diversion, spill diversion and equipment decontamination.

Major Trade Names

Envirosalv Poly-Overpack Salvage Drum

Envirosalv Poly-Overpack Salvage Drum

This unit is designed for handling, dispensing and disposing of costly hazardous materials. It is made of HDPE to resist flammable liquids, chemicals and corrosives. This drum features a lockable lid that offers added security, ensuring that the contents are not accessed by unauthorised personnel. I...

t also includes moulded-in handles for easy transport and a stackable design, allowing efficient use and storage space.

SteelPal Stacker Spill Pallets

SteelPal Stacker Spill Pallets

These pallets are used for moving drums safely and securely around the facility by a forklift. They are designed for storing two 55-gallon drums and feature steel sidewalls for security and spilling of contents during transportation. They can be stacked on top of one another for a convenient, portab...

le racking system.

Q-VAC Hazmat Vacuum

Q-VAC Hazmat Vacuum

This vacuum system is designed for safe and efficient cleanup of hazardous materials and spills. It features a powerful suction pump that is capable of removing hazardous materials from floors, surfaces and other areas. It also includes a spill scooter that allows easy mobility and manoeuvrability i...

n tight spaces. This unit has a liquid overflow shutoff valve to prevent liquid overflow or spillage by shutting off the flow of liquid once the level reaches a predetermined point.

ENSORB Wheeled Salvage Drum Spill Kit

ENSORB Wheeled Salvage Drum Spill Kit

The spill kit is designed to contain and clean up spills of hazardous materials and other liquids. It is contained in a polyethylene-wheeled salvage drum that allows easy transportation to the site of the spill. The kit contains absorbent materials that quickly soak up any spilt liquid (including wa...

ter), disposal bags & ties and PPE (gloves & goggles) to protect workers from exposure to hazardous materials.

Enpac Competitive Advantages

Bazooka Passive Oil Filter For Spill Containment

Bazooka Passive Oil Filter For Spill Containment

Bazooka oil filter spill containment unit is designed to be used in conjunction with spill containment berms to filter hydrocarbons, such as oil & gasoline from rainwater runoff or other spills. It features a trickle filter and an automatic shut-off valve using Drainiac technology to help capture oils and fuels while letting clean water pass easily...

. This unit also includes a pre-filter that swells as it absorbs hydrocarbons from entering the drain, causing any damage. The Bazooka system can be installed in a variety of locations, including stormwater drains, catch basins and other drainage systems.

Frequently Asked Questions

How to install the Enpac Bazooka system?

  • Determine the location for the Bazooka depending on the application needs. Always consider factors such as the type and volume of liquids flowing through the system, as well as potential sources of hydrocarbon contamination.
  • Remove any debris or sediments that may interfere with the installation process.
  • Install the Bazooka in the designated location and secure it in place using the provided mounting hardware.
  • Connect the inlet and outlet hoses to the appropriate ports on the Bazooka, making sure that they are properly secured and leak-free.
  • Test the Bazooka to ensure that it is functioning properly. This may involve running water or other liquids through the system and monitoring for any signs of hydrocarbon contamination or leaks.
  • Regularly inspect and maintain the Bazooka to ensure that it continues to function effectively..
  • Clean or replace the filter media, inspect the hoses and connections for damage and monitor the system for signs of wear or corrosion.

How to use the spill containment berm?

A.

  • Determine the appropriate size and type of berm needed for the material to be contained.
  • Clear the area where the berm will be placed of any debris or obstructions.
  • Place the berm in the desired location, making sure that it is level and centred.
  • Anchor the berm using stakes or other secure anchors.
  • Place the materials to be contained inside the berm.
  • If the berm has walls, make sure they are securely in place.
  • Monitor the berm frequently to ensure that it is containing the material effectively.
  • Clean up the spill or leak as soon as possible once it has been contained.
  • Dispose of the materials properly to prevent any damage to personnel and property.
  • What are the absorbent materials made of?

    The absorbent materials are made from a blend of recycled cellulose fibres and superabsorbent polymers that can absorb up to 20 times their weight in liquids. They include items like pads, pillows and socks for quick absorption and spill control.