CASH VALVE

The Cash Valve's extensive catalogue comprises relief valves, isolation valves, back pressure controls & regulators, air-operated valves, pressure build economisers and strainers. The brand's cryogenic valves are designed for regulating the pressure of liquified natural & compressed natural gas. They feature brass construction for withstanding pressures up to 700 psi & temperatures as low as -320 degrees Fahrenheit. These units have a compact design for ease of installation in confined spaces and are available in 3/8 and 1/2 inch pipe sizes. Cash air operated valves use air pressure to produce linear or circular movements to perform valve functions. They are available in normally closed and normally open valve configurations for safe flowing of the fluids on Raptor Supplies.

See More

Request a Quote

CASH VALVE Pressure Regulators

Pressure Regulators (4828 Products) Brass and bronze pressure control valves featuring a maximum operating pressure of 2400 psi. Can automatically stop liquid or gas flow at a factory-set pressure point

CASH VALVE Relief Valves

Relief Valves (112 Products) Used to control or limit pressure build-up in a system and have a maximum factory-set pressure of 1000 psi. Available in different body and disc materials

CASH VALVE Air Operated Valves

Air Operated Valves (11 Products) Use air pressure to produce linear or circular movements to perform valve functions. Available in normally closed and normally open valve configurations

Things To Consider

Cross-Reference Alternatives

Cash Valve's MPNs cross individual references to the equivalent Plast-O-Matic, Martins Industries and Blacoh Fluid Control model numbers. So, if you are looking for competitor items that are either out of stock or obsolete, chances are Raptor Supplies has the equivalent Cash regulators & valves available. Customers can also cross-reference most products using the last 5 digits of the model numbers.

Shipping

Cash regulators & valves are available in pressures ranging from 0 to 1500 psi. These valves and regulators are small & heavy in size & therefore require careful packaging as some products might get damaged while shipping. Hence, they are delivered by courier shipment and not air freight for minimum downtime.

About CASH VALVE

The Cash Valve's extensive catalogue comprises relief valves, isolation valves, back pressure controls & regulators, air-operated valves, pressure build economisers and strainers. The brand's cryogenic valves are designed for regulating the pressure of liquified natural & compressed natural gas. They feature brass construction for withstanding pressures up to 700 psi & temperatures as low as -320 degrees Fahrenheit. These units have a compact design for ease of installation in confined spaces and are available in 3/8 and 1/2 inch pipe sizes. Cash air operated valves use air pressure to produce linear or circular movements to perform valve functions. They are available in normally closed and normally open valve configurations for safe flowing of the fluids on Raptor Supplies.

Major Trade Names

KP Series Back Pressure Valves

KP Series Back Pressure Valves

These pilot-operated back pressure valves provide dependable protection and accurate control against overpressure conditions. They feature brass construction, stainless steel spring and Buna-N seat disc & diaphragm, allowing pressure setting from 15 to 200 psi.

LS High-Pressure Regulating Valves

LS High-Pressure Regulating Valves

These spring-loaded, single-seated, direct-acting diaphragm type regulators maintain decreased pressure within relatively close limits regardless of inlet variations. They include a spring chamber, bronze body, bottom plug, piston assemblies / stainless steel piston, seat ring, cylinders, strainer s ... creens, O-rings and Buna-N diaphragm. These units further allow reinstallation of the self-renewable seat ring by flipping it over rather than replacing it.

CASH VALVE Competitive Advantages

Floating Ring in Industrial Back Pressure Valves

Floating Ring in Industrial Back Pressure Valves

The unique full floating ring seating arrangement in the industrial back pressure valves ensures smooth and balanced control even during pressure changes. These regulators provide exceptionally close control, repeatability of opening pressure and close reseating pressures.

Frequently Asked Questions

Q. Where are Cash Valve products manufactured?

A. Cash Valve products are manufactured in Black Mountain, NC.

Q. Are Cash Valve products certified?

A. Yes, Cash Valve products are ISO 9001 certified.

Q. Where was Cash Valve Company founded?

A. Cash Valve Manufacturing Company was founded in Decatur, IL by A.W. Cash.

Q. How do pressure valves work?

A. The outlet pressure of the valve drives the diaphragm upward to close the valve at the bottom. When the outlet pressure falls below the valve's set point, the spring pressure takes over and pushes the valve stem downward, allowing the valve to open.

Q. Where should a back pressure valve be installed?

A. In general, the back pressure valve can be positioned anywhere in the discharge line as long as there is some downstream pressure at the dose point. To stop syphoning and drainage of the chemical line if there is no downstream pressure, the back pressure valve should be fitted at the dose point.