Authorized Distributor ofBEVEL TOOL

BEVEL TOOL

The brand's extensive catalogue includes router bits, bevelers, insert bearings, plate & plate covers and rotary brushes & pad drivers. Bevel Tools' aluminium bevel router heads have aluminium construction for structural rigidity and corrosion resistance. These router heads feature angled cutter heads for fine cutting and optimum performance. The brand's Bevel Mite pneumatic motor bevel tools have a pneumatic motor for enhanced performance. These tools feature a spindle locking button that enables changing the router head within 35 seconds. It has a freely rotating flange made of hardened (nitrated) steel for added strength.

See More

Request a Quote

Things To Consider

Cross-Reference Alternatives

Customers searching for the company's bevelling tools can look for the model, item or cross-reference number on our website. We also source direct alternatives for various old and discontinued products, with no minimum order quantity required for placing orders.

Shipping

These Bevel Tools products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.

About BEVEL TOOL

The brand's extensive catalogue includes router bits, bevelers, insert bearings, plate & plate covers and rotary brushes & pad drivers. Bevel Tools' aluminium bevel router heads have aluminium construction for structural rigidity and corrosion resistance. These router heads feature angled cutter heads for fine cutting and optimum performance. The brand's Bevel Mite pneumatic motor bevel tools have a pneumatic motor for enhanced performance. These tools feature a spindle locking button that enables changing the router head within 35 seconds. It has a freely rotating flange made of hardened (nitrated) steel for added strength.

Major Trade Names

Bevel Mate

Bevel Mate

Bevel Mite is a line of compact, handheld tools used for creating bevelled edges on various materials, such as wood, metal and plastic. It is designed to be used for precision cutting and shaping tasks, such as creating angles and chamfers on edges and corners. This tool is operated by using a high- ... speed rotating blade to cut the material at the desired angle. It is lightweight and easy to manoeuvre in tight spaces.

Bevel Mite

Bevel Mite

Bevel Mite machines are designed for easy and flexible use, with a weight limit of only 2 kg, making them light and easy to manoeuvre. These handheld machines are ideal for quick beveling, rounding, and deburring sheet metals. They provide faster weld preparation and consistent, high-quality results ... as they have solid carbide bevel heads offering long service life. With the Bevel Mite concept, you can achieve these results with minimum physical effort, making it a popular choice among professionals in the metalworking industry.

Frequently Asked Questions

Q. How do I choose the right router bit?

A. Choosing the right router bit depends on the type of material you are working with and the specific cut you want to make. It is important to choose a bit that is appropriate for the task at hand and that matches the size and shape of the cut you want to make.

Q. What is the difference between the brand's bevel guide and bevel tool?

A. A bevel guide is typically a stationary tool that attaches to a saw or router table. It provides a guide for the blade / bit to cut at a specific angle, creating a bevelled edge. A bevel guide is useful for creating consistent and precise cuts, particularly for larger workpieces or when working with materials that require a high level of accuracy. On the other hand, a bevel tool is a handheld tool used to create bevelled edges on metal, plastic and wood. It is designed for precision cutting and shaping tasks, such as creating angles and chamfers on edges & corners. A bevel tool is lightweight and easy to manoeuvre.

Q. How do I install Bevel Tools stainless steel flange heads?

A.

  • First, ensure that the flange head you are installing is the correct size and type for the task you are performing.
  • If necessary, remove the existing flange head from the beveling machine by unscrewing it counterclockwise.
  • Place the Bevel Tools stainless steel flange head onto the beveling machine's spindle and tighten it by turning it clockwise. Use a wrench or pliers if necessary to ensure a tight fit.
  • Once the flange head is securely attached to the beveling machine, insert the appropriate beveling blade into the flange head's mounting hole.
  • Make sure the blade is properly aligned and tightened according to the manufacturer's instructions.
  • Test the beveling machine to ensure that the flange head and blade are securely attached and working properly.